Previous topicNext topic
Help > User Interface > Modeling > Behaviors >
Rotational Actuator

Rotation Actuator Behavior

Basic Information

Name:The name of this behavior

Motor Device:Select the linkage controlled by this behavior

Motion:Adjust the angle of the controlled linkage

Velocity:Maximum speed percentage

Max Velocity:Maximum speed

Acceleration:AccelerationsAction Latency:Delay time after receiving the signal (not available in this version)

Control Mode

Acting Type:Select the mode to control this device

Digital Input Settings (Power-Control)

Digital Input-1:The first receiver device used by this behavior (forward/reverse rotation)

Channel-1:The channel corresponding to receiver device-1

Activate Level:Whether receiver device-1 is triggered by a rising or falling edge

Digital Input-2:The second receiver device used by this behavior (brake/release brake)

Channel-2:The channel corresponding to receiver device-2

Activate Level:Whether receiver device-2 is triggered by a rising or falling edge

The default control method is as follows:

Digital Input-1 Digital Input-2 Action
1 1 Forward rotation
0 1 Reverse rotation
1 0 Stop
0 0 Stop

Digital Input Settings (Single-Acting)

Digital Input:The receiver device used by this behavior (forward rotation/stop)

Channel:The channel corresponding to the receiver device

Activate Level:Whether the receiver device is triggered by a rising or falling edge

The default control method is as follows:

Digital Input:True:Forward rotation

Digital Input:False:Stop

Digital Input Settings (Double-Acting)

Digital Input-1:The first receiver device used by this behavior (forward/reverse rotation)

Channel-1:The channel corresponding to receiver device-1

Activate Level:Whether receiver device-1 is triggered by a rising or falling edge

Digital Input-2:The second receiver device used by this behavior (forward/reverse rotation)

Channel-2:The channel corresponding to receiver device-2

Activate Level:Whether receiver device-2 is triggered by a rising or falling edge

The default control method is as follows:

Digital Input-1 Digital Input-2 Action
1 1 Forward rotation
0 1 Reverse rotation
1 0 Stop
0 0 Stop

Advanced

Follower Device:Follower device (can select other follower linkages)

Transmission Ratio:Conversion ratio of movement distance between master and follower linkages

Follower Motion:Adjust the position of the follower linkage