Name:The name of this behavior
Motor Device:Select the linkage controlled by this behavior
Motion:Adjust the position of the controlled linkage
Max Position:Positive limit position
Min Position:Negative limit position
Velocity:Maximum speed percentage
Max Velocity:Maximum speed
Acceleration:Acceleration
Action Latency:Delay time after receiving the signal (not available in this version)
Acting Type:Select the mode to control this device
Digital Input-1:The first receiver device used by this behavior (forward/backward)
Channel-1:The channel corresponding to receiver device-1
Activate Level:Whether receiver device-1 is triggered by a rising edge or falling edge
Digital Input-2:The second receiver device used by this behavior (release brake/brake)
Channel-2:The channel corresponding to receiver device-2
Activate Level:Whether receiver device-2 is triggered by a rising edge or falling edge
The default control method is as follows:
| Digital Input-1 | Digital Input-2 | Action |
|---|---|---|
| 1 | 1 | Stop |
| 1 | 0 | Forward |
| 0 | 1 | Backward |
| 0 | 0 | Stop |
Digital Input:The receiver device used by this behavior (forward/stop)
Channel:The channel corresponding to the receiver device
Activate Level:Whether the receiver device is triggered by a rising edge or falling edge
The default control method is as follows:
Digital Input:True:Forward
Digital Input:False:Stop
Digital Input-1:The first receiver device used by this behavior (forward/backward)
Channel-1:The channel corresponding to receiver device-1
Activate Level:Whether receiver device-1 is triggered by a rising edge or falling edge
Digital Input-2:The second receiver device used by this behavior (forward/backward)
Channel-2:The channel corresponding to receiver device-2
Activate Level:Whether receiver device-2 is triggered by a rising edge or falling edge
The default control method is as follows:
| Digital Input-1 | Digital Input-2 | Action |
|---|---|---|
| 1 | 1 | Stop |
| 1 | 0 | Forward |
| 0 | 1 | Backward |
| 0 | 0 | Stop |
Follower Device:Follower device (can select other follower linkages)
Transmission Ratio:Conversion ratio of movement distance between master and follower linkages
Follower Motion:Adjust the position of the follower linkage