Previous topicNext topic
Help > User Interface > Modeling > Behaviors >
Camera

Camera Behavior

Basic Information

Name:The name of this behavior

Camera:Select the camera device

Exposure:Exposure time of the camera device

Interval:Frame update interval of the camera device

Image Overwrite:Whether to overwrite saved images, up to 1000 images can be retained

Save Folder:Path to save images

Response Time:Response time from input control signal to output processing result (not provided in this version)

Action Latency:Delay time after receiving the signal (not provided in this version)

Camera Setting

Field of View:Camera field of view

Width:Camera image width

Height:Camera image height

Near Threshold:Nearest visible distance of the camera

Far Threshold:Farthest visible distance of the camera (set to 0 for infinity)

Focal Plane:Position of the sharpest image (set to 0 for clarity within the visible range)

Depth of Field:Camera depth of field, 1~infinity, the larger the value, the deeper the depth of field

Setting 0 means clarity within the visible range

Setting Depth of Field to 100 does not mean a depth of field of 100mm; the depth of field range is calculated internally by the system

Digital Input Setting

Digital Input:Receiver device used by this behavior

Channel:Channel corresponding to the receiver device

Activate Level:Whether the receiver device is triggered on a rising or falling edge

The default control method is as follows:

Digital Input:True:Start capturing

Digital Input:False:Stop capturing

Advanced

Enable Indicator:Whether to use the LED device for this behavior

Indicator:Select the LED device for this behavior

Engaged Color:Color when the camera is saving images

Disengaged Color:Color when the camera is idle (not saving images)