Previous topicNext topic
Help > User Interface > Modeling > Behaviors >
Reed Switch

Reed Switch Behavior

Basic Information

Name:The name of this behavior

Sensor:Select the Connector device for this behavior

Sensing range:Sensing distance

Type:The trigger type of this behavior

Action Latency:Delay time after sending the signal (not available in this version)

The connector device must meet the following table to appear in the dropdown menu:

Device Setting
Type Active
Connector Setting
Is Locked False
Auto Lock False
Snap False

Digital Output Setting

Digital Output:The transmitter device used by this behavior

Channel:The corresponding channel of the transmitter device

Activate Level:The trigger state of the transmitter device

Parameter default value changes (after DIATwin v0.1.17):

Activate Level:High:Low

Therefore, the value of Activate Level in DTL files saved by older software versions will be changed when read by the new version:

High = Low;Low = High

Advanced

Enable Indicator:Whether to use the LED device for this behavior

Indicator:Select the LED device for this behavior

Engaged Color:The color when the behavior is triggered

Disengaged Color:The color when the behavior is not triggered

The LED device must have more than one color to appear in the dropdown menu