Previous topicNext topic
Help > User Interface > Modeling > Behaviors >
Micro Switch

Micro Switch Behavior

Basic Information

Name:The name of this behavior

Sensor:Select the collision sensor device for this behavior

Type:The trigger type of this behavior

Action Latency:Delay time after sending the signal (not provided in this version)

Digital Output Setting

Digital Output:The transmitter device used by this behavior

Channel:The corresponding channel of the transmitter device

Activate Level:The trigger state of the transmitter device

LED devices with more than one color will appear in the dropdown menu

Parameter default value changes (after DIATwin v0.1.17):

Activate Level:High → Low

Therefore, the Activate Level value in DTL files saved by older software versions will be changed when read by the new version:

High → Low; Low → High

Advanced

Enable Indicator:Whether to use the LED device for this behavior

Indicator:Select the LED device for this behavior

Engaged Color:The color when the behavior is triggered

Disengaged Color:The color when the behavior is not triggered

LED devices with more than one color will appear in the dropdown menu