Previous topicNext topic
Help > User Interface > Modeling > Behaviors >
LED

LED Behavior

Basic Information

Name:The name of this behavior

Indicator:Select the LED device for this behavior

Engaged Color:The color when triggered

Disengaged Color:The color when not triggered

Response Time:The response time from input control signal to output processing result (not provided in this version)

Action Latency:The delay time after receiving the signal (not provided in this version)

Digital Input Setting

Digital Input:The receiver device used by this behavior

Channel:The corresponding channel of the receiver device

Activate Level:Whether the receiver device is triggered on a rising edge or falling edge

The default control method is as follows:

Digital Input Status Color
True Triggered Color-1
False Not Triggered Color-2