Name:The name of this behavior
Spot Light:Select the spotlight device for this behavior
Color:The color of the spotlight
Intensity:The intensity of the spotlight
Beam Width:The beam width of the spotlight
Beam Width:Must be less than or equal to the Cut Off Angle
Cut Off Angle:The tilt angle of the spotlight
Action Latency:Delay time after receiving the signal (not provided in this version)
Digital Input:The receiver device used by this behavior (turn on/off the light source)
Channel:The channel corresponding to the receiver device
Activate Level:Whether the receiver device is triggered on the rising edge or falling edge
The light source behavior settings must comply with device specifications to avoid exceeding the range.