Previous topicNext topic
Help > User Interface > Modeling > Behaviors >
Conveyor

Conveyor Behavior

Basic Information

Name:The name of this behavior

Motor Device:Select the Track device for this behavior

Velocity:Maximum speed percentage

Max Velocity:Maximum speed

Acceleration:Acceleration

Action Latency:Delay time after receiving the signal (not available in this version)

Acting Type:Select the mode to control this device

Digital Input Setting (Power-Control)

Digital Input-1:The first receiver device used by this behavior (conveyor forward/reverse)

Channel-1:The channel corresponding to receiver device-1

Activate Level:Whether receiver device-1 is triggered on rising or falling edge

Digital Input-2:The second receiver device used by this behavior (conveyor brake release/brake)

Channel-2:The channel corresponding to receiver device-2

Activate Level:Whether receiver device-2 is triggered on rising or falling edge

The default control method is as follows:

Digital Input-1 Digital Input-2 Action
1 1 Conveyor forward
0 1 Conveyor reverse
1 0 Stop
0 0 Stop

(The device is initially in a brake state, and Digital Input-2 must first release the brake before controlling the device)

Digital Input Setting (Single-Acting)

Digital Input:The receiver device used by this behavior (conveyor forward/stop)

Channel:The channel corresponding to the receiver device

Activate Level:Whether the receiver device is triggered on rising or falling edge

The default control method is as follows:

Digital Input:True:Conveyor forward

Digital Input:False:Conveyor stop

Digital Input Setting (Double-Acting)

Digital Input-1:The first receiver device used by this behavior (conveyor forward/reverse)

Channel-1:The channel corresponding to receiver device-1

Activate Level:Whether receiver device-1 is triggered on rising or falling edge

Digital Input-2:The second receiver device used by this behavior (conveyor forward/reverse)

Channel-2:The channel corresponding to receiver device-2

Activate Level:Whether receiver device-2 is triggered on rising or falling edge

The default control method is as follows:

Digital Input-1 Digital Input-2 Action
1 1 Conveyor forward
0 1 Conveyor reverse
1 0 Stop
0 0 Stop

Relevant Notes for Use

The conveyor movement direction is along the +X axis of the coordinate system