DIATwin is a platform that helps equipment manufacturers and production line integrators develop and test machines in a virtual setting. Using digital twin technology, it allows users to fully check and optimize machine functions, paths, and processes before they are built in the real world. This "test first, deploy later" approach leads to less time spent on troubleshooting and maintenance, reduces risks during implementation, and ensures that machines are fully ready to perform optimally before they are shipped out. As a result, this speeds up production times, increases quality, and helps companies get up and running faster.