Preferences
3D Rendering
| Wireframe Mode |
In wireframe mode, the edges of objects are displayed with black lines. |
| Shading Mode |
In shading mode, the black edge lines of objects are turned off. |
| Outline Mode |
Only the outline of objects is displayed, and the rest is transparent. |
Display
| Show Coordinate Axes |
Allows users to show or hide the world coordinate axes, helping them understand the orientation of the model
in 3D space. |
| Show All Boundary Outlines |
Allows users to show or hide all established boundary outlines, helping them determine if the model has
boundary outlines. |
| Show Connector Axes |
Allows users to show or hide all established connector axes, helping them observe if the connector orientation
is correct. |
| Show Joint Axes |
Allows users to show or hide the axes of established rotational joints, helping them observe if the axes are
in the correct position. |
| Show 3D Camera Frustum |
Allows users to show or hide the field of view of established 3D cameras, helping them verify if the current
camera settings are correct. |
| Show Camera Frustum |
Allows users to show or hide the field of view of established 3D cameras, helping them verify if the current
camera settings are correct. |
| Show Distance Sensor Rays |
Allows users to show or hide the rays of distance sensors, helping them observe if the direction and distance
of the sensors are correct. |
| Show Light Sensor Rays |
Allows users to show or hide the rays of light sensors, helping them observe if the direction of the light
sensors is correct. |
| Show Light Position |
Allows users to show or hide the position and orientation of lights, helping them observe if the lighting
direction is correct. |
| Show Pen Painting Rays |
Allows users to show or hide the rays and distances of brushes, helping them observe if the brush orientation
is correct. |
| Show Center of Mass |
Allows users to show or hide the mass distribution to further assess the stability of the structure. |
| Show Device Viewport |
Allows users to show or hide the image window, helping them verify if the current camera settings are correct.
|
| Enable Shadow Rendering |
Allows users to enable or disable shadow rendering. Shadow rendering effects can only be displayed if shadow
casting is enabled in the default light source settings of the environment lighting. |
Settings
| Interface |
Allows users to set the display language of the user interface and the Python program path. |
| Environment Lighting |
Allows users to add or adjust the orientation and brightness of environment lighting. |
| Floor Settings |
Allows users to adjust the size, color, grid, and other settings of the floor. |
| 3D World Background Settings |
Allows users to customize the background color or background image. |
| Dragger Settings |
Allows users to set the dragger move increment and rotation increment. |
Account
Users can set the manufacturer and author names here.
This information will be included in the advanced settings
when saving files.