Name:The name of this behavior
Reference Node:Select a general frame as the material source point
Source From:Choose the source of the component
Acting Type:Select the operating mode of the device
Layout:Select the Component in the current world as the material
File Path:Select the full path of the .dt file to generate the Component
The selected .dt file will be packaged together when saving
Time Interval:Generates a component at a specified interval
Digital Input:The receiver device used by this behavior (Start material generation / Stop material generation)
Channel:The channel corresponding to the receiver device
Activate Level:Whether the receiver device is triggered on a rising edge or falling edge
The default control method is as follows:
Digital Input:True:Start material generation
Digital Input:False:Stop material generation
Digital Input:The receiver device used by this behavior (Generate material / No function)
Channel:The channel corresponding to the receiver device
Activate Level:Whether the receiver device is triggered on a rising edge or falling edge
The default control method is as follows:
Digital Input:True:Generate material
Digital Input:False:No function